I simulated 3V3 regulator with model LM63625DQPWPRQ1 that schematic is attached with this query. In that I have raised the input voltage from 5.786 V to 24 V. During line regulation output ripple current is continuously varying(sometimes enters into discontinuous conduction mode) which not expected as per my design. And switching voltage also getting some disturbance. I also attached the result which I have facing issues. Kindly provide the possible solutions.