Other Parts Discussed in Thread: SFRA
Dear team:
The customer's test is added as BUILD 3, when DC_CHECK is 0
// BUILD 3 Voltage loop with inner current loop #define INCR_BUILD 3
// Check system under DC condition (cleanest SFRA curves) 0 is FALSE, 1 is TRUE #define DC_CHECK 0
For a fixed inverter output (that is, the inverter output is always kept at 220V), is the value of invVoRef a fixed value or a changing value?
Best regards