This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSLCDK6748: Enquiry about signal transmission.

Part Number: TMDSLCDK6748


Hello there,

I have to transmit a video using COFDM modulation, so I need at least 8Mhz of bandwidth, small form factor.

TMS320C6748 looks good for my application.

If I want to use this along with TMDSLCDK6748, is there any possible way to integrate the transceiver module with the DSP so that as I get the output in COFDM  I can transmit it using the RF transceiver at my receiver station?

Basically, Can I directly integrate the AFE79-LMH9-EVM Evaluation Module with OMAP-L138/C6748 Low-Cost Development Kit (LCDK)?


Thanks

Mohit