Hi,
what materials were used for the transformer and inductors in PMP22650 eval board?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
what materials were used for the transformer and inductors in PMP22650 eval board?
Hi User,
Thanks for reaching out! Can you confirm which transformers and inductors you're referencing with the reference designators? I'm assuming you mean the Cyntec power stage transformer. Which inductors are you referring to? Are you looking for the datasheets? If specific material construction like core and stackup, it would be good to get the details from the magnetic vendors as these are typically proprietary info. Thanks!
Hi Darwin,
Thank you for the quick response. You are right, I mean the CLLC power stage transformer T1 . I guess, this is a custom component, that's why I wasn't able to find any information about this component on Cyntec website. I would like to know what material was used for transformer core, for example 3C96 or 3F3. The same information for T2 and T3.
Thanks!
Hi User,
For this proprietary information, I recommend reaching out to the magnetic vendors directly as TI wouldn't be able to share this kind of information. If unable to get a hold of the magnetics vendor through their website, let me know and we can try and find the right vendor contact for you. Thanks!