Part Number: PMP9087
Hello,
I am planning to modify the PMP9087 design for an input voltage 110Vdc - 200Vdc to 5V output and output current of 500mA. Need clarification on the design modification required other than feedback resistors.
Also want to understand if there is any limitation in the meeting the specification (such as duty cycle etc.)
Regards,
Anand Meharwade