Dear Texas tech team,
I was referring your TIDA-01605 document, In that I could not understand the topic (2.3.2.3 Two-Level Turnoff Protection - page no :10).
I know it is just a reference design and I should take it for only obtaining basic details but As a customer that basic details itself is missing in that topic. For example, Kindly clarify the following questions
1. There is not mentioned where is the V_terminal point? But I assumed that it is the point at capacitor C25. Because the voltage equation given in the topic tells the voltage division.
If it is so, Here comes another question What is the impact of C25 capacitor?

2. How gate capacitor can discharge through C25 Capacitor? (As per my point of view voltage at C25 cannot be 11.9V it must be 15V only)
3. As per the topic, the voltage at point C25 is 11.9V. If it is true then how it reached 5.5V?

Dear team, I don't know whether the topic contains any wrong information or not. But as a customer, I need at least basic clarification which is missing in that topic. So kindly clarify the basic clarification as soon as possible.
Hoping a warmful reply from TI. Thank you team!