Hi team,
My customer would like to know,
TIDA-01606 is using SVPWM to control?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
My customer would like to know,
TIDA-01606 is using SVPWM to control?
Hi Jason,
currently, in the TIDA-01606 there is no SVPWM modulation implemented when you run the power.
There is a function that allows you to implement the space vector (TINV_updateSVPWM) but without DC bus middle voltage balancing control I do not recommend the customer to run it.
Thanks for your attention
Best Regards
Riccardo
Hi Riccardo,
Thanks for your sharing, and my customer still have two question, could you please help.
Customer would like to know if there is no SVPWM, which modulation TIDA-01606 used?
Customer doesn't find TINV_updatesSVPWM in TIDA-01606 project, could you tell me where could find it?
Jason
Hi Jason,
currently, the output of the PI Controller after the transformation is directly giving you the duty cycle, which will be sinusoidals. These duty cycles are constrained between 1 and minus 1.
There is no third harmonic injection, space vector modulation etc. implemented in the code.
In the code of TIDA 01606, there is a function mentioned called TINV_updateSVPWM in the file: tinv.h.
The function is located close to row 711.
Thanks for your attention
Best Regards
Riccardo