Hello,
I have come across TIDM-02000 reference design for implementing Peak Current Mode Controlled PSFB converter using F280049. I need to order magnetic components such as transformers and inductors specified in the BoM. Can anyone provide direct contact details of the person in the manufacturing company who handles these parts? Following are the part details:
Part Details | Manufacturer | Part No. |
12:1, Center-tapped, Main Power Transformer | MPS | P6524_A |
Inductor, 4.7uH | Vitec Electronics Corp | 6193R |
Inductor, 39uH | Vitec Electronics Corp | 6194R |
Thanks in advance.