This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-00643: How to reduce power consumption when motor is not running ?(System is disabled)

Part Number: TIDA-00643
Other Parts Discussed in Thread: DRV8305

I am working on Instaspin ProjLab5b.

The hardware is TIDA_00643.

The Supply voltage is 12V. It is battery operated. 

The power consumption when motor is not running and enable is reset to 0(zero) is 120mA. How can I reduce the power consumption ?