This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDM-1000: AC input and output issue

Part Number: TIDM-1000

Hi team,

Here's an issue from the customer may need your help:

The AC input in datasheet is 400 VL-L 50 Hz, Output 700-V DC Nominal. Is derating possible like input AC 220VL-L 50 Hz, output DC 400V DC Nominal. And can it be adjusted by modifying the parameters in the program?

Could you help check this case? Thanks.

Best Regards,

Cherry

  • Hi Cherry,

    We only suggest to run under the condition in the user guide. I can only say that it might work with the change of the code but the performance might not be very good due to the sensing ratio etc. 

    Regards,

    Chen