Hi EXpert,
I have some questions about below description.
- "When the AC input changes from the positive half line to the negative half line at the zero-crossing, theduty ratio of the low-side high-frequency switch SiC2 changes from 100% to 0%, and the duty cycle of SiC1 changes from 0% to 100%. " Why the PEM duty for SiC is 0% or 100%? I suppose they are not 0 or 100% when normal working.
- "Because of the slow reverse recovery of the high-side diode (or body diode of the MOSFET), the voltage at the cathode of D2 cannot jump from ground to DC+ voltage instantly (this causes a large current spike)." I can understand the issue cause. But I suppose we need to improve D1 and D2 reverse recovery. Why the solution becomes change S1 and S2 to SiC or GaN? Is these related? Thanks.
BR,
Elec Cheng