Other Parts Discussed in Thread: SM72295,
Hi,
I have used the reference design TIDA-00365 to design motor controller for brushed DC motors, I ran the motors with 16KHz PWM signal via SM72295 and through the H-Bridge at different duty cycles.
My observations are that upto 90% duty cycle the output is a nice square wave but above 90% duty cycle the output of the H-Bridge starts to become noisy, I am not able to understand why this is occurring, is this some kind of limitation with this design?
here the reference schematic, Q6 highlighted in RED.

CH-1 is Gate of n-CH Mosfet Q6
CH-2 is source of n-CH Mosfet Q6
Math: CH2 - CH1
here is the output at 90% duty cycle nice square wave in RED

Here is the output at 93% duty cycle, poor quality and noisy square wave in RED