This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDM-RF430-TEMPSENSE: PCB Manufacturing

Part Number: TIDM-RF430-TEMPSENSE
Other Parts Discussed in Thread: RF430FRL152H

PCBWay manufacturing options

Hello,

I would like to manufacture the reference design TIDM-RF430-TEMPSENSE from PCBWay as a Flexible Polyimide PCB. However, I'm not sure which options I should select. Could you please give advice for the following manufacturing options? In addition, should the drill layer be made as A.Tenting vias, B.Plugged vias, or C.Vias not covered?
Thanks!

  • Hello Vivian,

    I'm glad to see your interest in the TIDM-RF430-TEMPSENSE reference design. These kind of manufacturing information is not available. Maybe it is possible to extract some of these information from the provided Gerber files or the CAD symbols. I also believe that these manufacturing parameters are not so critical for the RF430FRL152H device functionality. They rather depend on reliability and environmental aspects of your application, on which TI can not give a judgement.

    Best regards,

    Andreas.