Can you please provide the alternate part number for the Wurth transformer 750318938? Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can you please provide the alternate part number for the Wurth transformer 750318938? Thank you.
Hi Christ,
I saw the picture of TIDA-050045 and it seems there is a LinkCom transformer as an alternative part.
I have sent an email to Linkcom for more information of datasheet and stock. I will get back to you when I receive their reply.
Best regards,
Diang
Hi Christ,
Thanks for your waiting. I got the reply from LinkCom. LPD0023-50R could be an alternative part if you want to keep the 5-V output voltage.
Output: 750318938 is 5V/12A; LPD0023-50R is 5V/14A.
PRI voltage: 750318938 is 36-72V, 250kHz; LPD0023-50R is 33-57V, 250kHz.
Auxiliary output: 750318938 is 13V/20mA; LPD0023-50R is 12V/50mA.
They have the same pin order and pin configuration, but the pad layout dimension are different.
750318938 pad layout:
LPD0023-50R pad layout:
LinkCom would like to know how many pieces of transformer you are looking for. And they have 12V/5A output transformer as alternative too. Please let me know if you have any questions or if you need more details.
Best regards,
Diang
Hi Christ,
I will close the thread for now.
If you need further help, please reply to my email (d-xing@ti.com) and I will be glad to help.
Best regards,
Diang