Hİ
I am using TIDA-00792 referance design . I notced that C2 capacitor voltage range is low. I thinking, C2 boostrap capacitor connected to directly to battery BAT+ pin . Battery voltage is 29.4 voltege for li-ıon on charge, but use of capacitor voltage range 25V , that is exceed. This is not true. Also C2 capcitor position on pcb is horizontal . this is cause a lot of stress on capcitor when PCB mounted.