Does TIDA-00915 apply three phase with neutral applications?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Xiaonan,
Thank you for the question.
TIDA-00915 is a design using 200V~400V DC input.
For AC inputs, external rectifier stage and bulk capcaitor in the DC bus are needed. Make sure the rectified DC bus voltage do not go beyond this 200V~400V range, then it can work.
Best regards,
Jerome Shan