HI TI Experts
In TIDA-0038,the PWR050A written that the VIN_MON 400V=1.93V,but in the PWR050A SCH ,that written 400V=1.5V,Please help me to make sure which one is right? How to calculate the VIN MON GAIN? Thank you !
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI TI Experts
In TIDA-0038,the PWR050A written that the VIN_MON 400V=1.93V,but in the PWR050A SCH ,that written 400V=1.5V,Please help me to make sure which one is right? How to calculate the VIN MON GAIN? Thank you !
I'll forward this to our expert.
Hello,
VIN_MON 400V=1.93V is based on ideal calculation with ideal sampling and hold. But the circuit averages input voltage with DC value, 1.5V corresponds to 400Vin actually.
Regards,
Sean
Hello,
I expect VIN_MON = 1.12V when Vin = 300V.
Regards
Hello,
Here is the aux transformer turns ratio. The transformer part number is GA358. Pri:Sense = 1:0.079. Another voltage divider is from: R16 and R14. N = R14/(R14 +R16). Then you can calculate the sensed voltage,