This is getting old. This is the fifth time I have written. No relevant reply yet.
Why was #4 cancelled?
The original error using Pspice for TI was
orcap 15092 orcommn 2302 proj-pspicefiles\schematic1\bias.sim orcommn 2302 cant initialize profile
Today I got an error that flashed on too fast to read: orsrvr 2004?
and orcap 15030: the Pspice com wrapper error has occurred.
New error: orcap 2328 opj file not loaded yet.
I got an email saying I did not have Pspice for TI [which is wrong]. When queried the version shows:
17.4-2022 s008 win spb 64 bit edition