This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMP30600-TH: withstand 75 V continuous input?

Part Number: PMP30600-TH
Other Parts Discussed in Thread: LM5146, LM5146-Q1-EVM12V

Hi all, I need a design that has a 10V-75V input range and can output 5V 10A (and more for Amps). Can I apply 75V continuous input for the reference design of the PMP30600-TH?