Other Parts Discussed in Thread: UCC28950
Hi Team, seeking some support for a customer.
PMP8740 and specifically "PMP8740 2KW Rev_E Full Bridge - Schematic.pdf" in tidm224. I want to modify it to have a 10V 200A output, what modifications do I need to make specifically?
T7, L3 what values would they take?
I'm also checking slua287.pdf.
I wonder if I can insert in PMP8740 what is explained in slua287.pdf. Can I do this or is this a scheme for low power applications? it would be useful to me because it would make it easier for me to make the T4 transformer by hand.
being able to do so, what value would L1 and L2 have on page 4 of slua287.pdf?
Thank you in advance.
-Mark