This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-01573: Driving Pulsed diode with 100ns pulse, 10A current and 0.1 duty cycle

Part Number: TIDA-01573
Other Parts Discussed in Thread: LMG1020

Hi Team,

I would like to know if the TIDA-01573/LMG1020EVM will be suitable to drive Hamamatsu Pulsed Laser Diode L11348-307-05. The device spec is punctured below:

I check the TIDA-01573 and it was capable of delivering 60A 1ns current pulses. What should be modified in the design to make this suitable for 10A 100ns pulse?

If not suitable, can you recommend other devices?

Thanks in advance.

Regards,

Marvin