Other Parts Discussed in Thread: TPSI2140-Q1
Hello Ti,
The addendum of TIDA-01513 application note provides the two-point isolation leakage error detection and also can calculate the Risop、Rison.
The method can meet the ISO6469-1 for get the each terminal to chassis resistance value.
In the ISO6469-1 standard also have define that the measuring device used in this test shall have an internal resistance above 10 M ohm.
But the simulation example of TIDA-01513 addendum that the internal resisatance not meet the internal resistance define.
Do you know the internal resistance design for the isolation resistance design is the must be meet requirement?