This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMP22220: development questions

Part Number: PMP22220
Other Parts Discussed in Thread: UCD3138,

Hi,

We would like to understand if and how to verify the code is properly compiled before uploading to UCD3138. We would like to minimize the risk of damaging the Hardware as it controls high power devices.

1. Is the project settings correct? It can only be built with "Arm7 device" and Optimization level set to 3.  It will fail to build with "UCD3138" / optimization level 2(default setting).
2. We will keep most of the original design from PMP22220 besides fan changing. Where is the fan control/setting block in source code? Where to set the voltage controlling?