Other Parts Discussed in Thread: AWR1642BOOST, AWR1642
Hi Experts,
I want to test TIDA-01570 with mmWave Demo Visualizer.
Is the bin file which write into TIDA-01570 the same as that of AWR1642BOOST (xwr16xx_mmw_demo.bin)?
if yes,
According to the circuit diagram,the pin F14 & H14 changed from AR_MSS_LOGGER , AR_BSS_LOGGER to CAN_FD1_RX , CAN_FD1_TX.
Do I need to adjust the code?
I connect the pin F14 to the Rx connector of UART to USB as a data port , the pin 6 & 8(AWR_RS232_TX & AWR_RS232_RX)on the J4 component are used as user port.
The test result shows mmWave Demo Visualizer can recognize awr1642 through user port , but can't connect to data port.
Which pin can be used as data port for testing purposes on TIDA-01570 ?
Thanks!