Other Parts Discussed in Thread: TIDA-01606
Dear TI team,
Good morning.
In voltage sensing calculation in Tida-00555,below calculations are considered.
Voltage to be sensed=230V
Add 20% to 230V That is 276(As per Tida-00555)
1. why 20% is being added?
Then 276VRms value converted to Vp-p value by multiplying 1.414
That is (276*1.414)=390V(As per TIDA-00555)
2. Why we need to convert RMS value to peak to peak value?
3.Do we need fallow above procedure for shunt type current sensing also?
A. Is above theoretical calculations applies for practical calculations also?
B. How good above calculations are when comparing with practical results?
C.Kindly share results document comparing theoretical and practical values if TI team having (Tida-01606 or any other reference design involving voltage sensing and current sensing)?
3.Do we need to convert IRMS to Ip-p in current sensing application calculations?
We need above details to accurately calculate and simulate in AC voltage and current sensing (Shunt )applications.
Kindly do the needful.
Thank you,
Girish Kantharaju