Other Parts Discussed in Thread: DRV8323
Hello,
I am trying to understand the functionality of using R27, R29 and R32 in TIDA-00774 application note page-2. Normally, I would connect INHx directly to MSP430 IC.
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I am trying to understand the functionality of using R27, R29 and R32 in TIDA-00774 application note page-2. Normally, I would connect INHx directly to MSP430 IC.
Thanks.
Hi YASA,
In fact, this is a low-pass filter composed of RC to avoid some noise in PWM. Not used in this design.
Thanks
Jenson
Hello Jenson,
Thank you for your fast response. I did not see Capacitors on the same design. Moreover, they do not put these resistors to all 6 gate signals. That is why, I confused :)
Hi YASU,
Sorry for my misreading, the RC I was referring to was R25/C46. For this design, support 1xPWM mode, so we can use HA , HB,HC input to DRV8323, that's why we put R25/C46.... in here, and also when we use 1xPWM mode we need to disconnect pwm to INHx, so that why we put R27/R29/R32 here,when use 1xPWM mode, we can remove the pwm control for these pins.
I hope this help.
Thanks
Jenson