Hi
I set 22nF between pin10 and Gnd.
Try the current limit about sereval times and I find out the LM25088 doesn't work, no more PWM signal, keep about 3V(DC).
Meter the pin15 and pin13 only 2K ohm.
I don't know how to do.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
I set 22nF between pin10 and Gnd.
Try the current limit about sereval times and I find out the LM25088 doesn't work, no more PWM signal, keep about 3V(DC).
Meter the pin15 and pin13 only 2K ohm.
I don't know how to do.
Hi
I use LM25088-2, I use the RES function now.
There is a new problem.
I find the DFC would change the frequency three steps.
At the three steps boundary, the PWM would be very unstable.
In my opinion, that is the root cause.
How could I do to make DFC very smooth?
Thanks.
Hi
I set the R-Shunt to 0.1ohm.
In the stead state 28V/06A, the RES pin raised itself.
I set the R-Shunt to 0.022ohm, I try to add the load to 28V/2.5A, the RES pin keep 0V
I think the reason is DCM.
Is that right?
Hi
3. Externally Controlled Hiccup: The RES pin can also be used as an input. By externally driving the pin to a
level greater than the 1.2-V hiccup threshold, the controller is forced into the delayed restart sequence. For
example, the external trigger for a delayed restart sequence can come from an overtemperature protection
or an output overvoltage sensor.
I try this function, give a extenal singal from current mirror voltage level, and the LM25088 was broken now.
Ripple, Iin & RES
Hi
It looks like not a nice DFC function.
Fisrt, once DD works into CCM, the Vout would dropout voltage lower related Iout.
Second, if 28V/2A works all DCM, the DFC in the two boundary (1/3 & 2/3 load) would shake.