This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMP30285: Selection of Transformer for PMP9204 Solution

Part Number: PMP30285
Other Parts Discussed in Thread: PMP30164, PMP20001

Hi

S.No Reference Design      Working Input Range  Transformer 
1     PMP30285        120-437 VAC 750317049
2     PMP30164        140-274 VAC 750316585
3     PMP20001.1         185-260VAC 750316002

I have some question on below point as Per reference design PMP9204.

1. Can you converter PCB(PMP9204) File to Gerber File.

2.Can I use Transformer 7508111111(EVM 28740) instead of RLTI-1067 in PMP9204

3.Can I use Transformer 750317049 or750316585 or 750316002(As per above reference design table) instead of RLTI-1067 in PMP9204

4.As Above reference design,  This solution Can work 85-264 VAC(Input) and 5VDC/2A(Output)

5.As Above reference design,  This solution Can work 75-264 VAC(Input) and 5VDC/2A(Output)