This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-010054: TIDA-010054 dynamic output voltage

Part Number: TIDA-010054

Does the software/hardware of TIDA-010054 support dynamically changing the voltage on the secondary?

If so, can you point me out to the relevant section in the software which handles selecting the output voltage.

Kind regards

Dean

  • Hi Dean,

    Currently the voltage reference is a fixed reference. You can easily change this by modifying the reference voltage dynamically.

    The variable to be modified is DAB_vSecRef_Volts which is available in ISR2 and gets initialized in DAB_initGlobalVariables

    Thanks and regards, Pawan