Part Number: PMP22343
Following PMP22343 design I have built a board for 12V to +/-30V conversion. During testing when i am powering up the circuit through a Keysight bench lab power supply DC at 12V with a 1,5A max CC current limitation it is immediately going to CC limit without any load at the output. EN pin is tied to GND at boot, when TPS turns on it goes into CC mode.
I have read Sanjay Kandula's post regarding same problem she had but the post doesn't show any solution apparently.
Please help me where to investigate.
Here the schematic I have used, following slavishly the design rules at https://www.ti.com/tool/PMP22343
Best regards