Other Parts Discussed in Thread: THP210, OPA320, LM7705
Hello, I want to design an iepe sensor signal conditioner. This signal conditioner that I will design will not include gain and attentautor parts. The signal from the iepe sensor will pass through the coupling capacitor and then pass through the low pass filter(gain :1 . After filtering the signal, this low pass filter will convert the single ended signal to a differential ouput signal and give it to the ADC input.
When I make the configuration in the picture and apply a 10khz +-1 V signal, I can get a differential signal with a slight phase shift.
-------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
However, when I put a coupling capacitor at the beginning and add 12 volt dc offset to the ac signal, it does not filter the offset(hp filter with coupling cap) and I get a result like this? I'm having a hard time understanding where my mistake is.
A second question: Is there a phase shift after the tida-01471 reference design passes through the low pass filter?
Can you help me with my design, thank you.