Part Number: PMP10733
Other Parts Discussed in Thread: TPA3251, , PMP22343, TPS54560
Hello all,
i'm designing a supply structure to supply both the TPA3251 VDD as well as the preamplifiers OP-Amps.
Therefore the output requirements of the supply converter structure are: +12V with ~100mA Current, Tolerance Band is 11 - 13V, and an opposing negative voltage at -12V with <50mA current (only OpAmp Supply and Drive, Tolerance only affects opamp output capability, so lets assume -10 .... -15V is OK)
Input Voltage is 10 - 36V, hence using a flybuck is off the table. It seems a stacked buckboost might be a good choice. Similar to the PMP10733 i plan to use a 1:1 coupled inductor (1:1 not 1:1:1!), yet i'm concerend the negtive output voltage is regulated well, but the positive output voltage will not be.
--> The idea overall is to regulate the positive output even with an inverting buckboost. Is there any good idea on how to do that? i do not want to use a post-reg for the +12V due to size and cost constraints.
If there is any other better idea for supply structure, i'm open for it ;)
Thanks,
best regards,
Lukas