This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Error while producing a report in FilterPro

Hello, I'm trying to generate a project report in FilterPro but the software gives me an error message under a PC with Windows 10 Pro. How can I solve it? attached screenshot of the error message....

TIA

error: "Failed to load design report. Cannot create object of type "System Windoiws.ResourceDictionary". Create instance failed, which can be caused by not having a public default constructor for System.Windows.resourceDictionary". error at object "System.Windows:Documents.FixedPage": Line 1 Position 198.

Help !