Other Parts Discussed in Thread: OPA320, , AMC1301, TLC372, LM393, OPA2350
HI everyone!
I would be happy if you take a time and answer these questions :
Q1: In "TIDA-00366 => TIDUBX1B.PDF => page 17 => Figure 13. Differential-to-Single Ended Signal Conversion" instead of OPA320 ( U5 ) shall we use OPA2350AU?
Q2: the NTC thermistor in IGBT module is electrically separated from all high voltage pins and it is somehow Isolated , so why we need to use AMC1301 or any other kind of Isolation?
Q3:in TIDA-00366 => TIDUBX1B.PDF => page 20 =>4.7.1 Selection of Comparators says:
"
A typical industrial drive needs to have overload protection to operate within 300 to 500 ns. The TLC372
helps reach this goal. The TLC372 is very low cost and a dual-channel comparator. It operates from a
supply range from 3 to 16 V and has a typical response time of 200 ns."
as far as I know most in IGBTs Short circuit capability is 10us , so why we need fast reaction op amp for overload protection around 300 to 500 ns, why we can not use LM393 with response of 1.5us?
thanks for your attention!
regards.
dave.