This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR50410: PSPICE Simulation Fail

Part Number: LMR50410

Hi All,

I am trying to simulate the circuit that produces +5VDC and +12VDC output in the PSpice. I performed the calculations for these circuits via WEBENCH POWER DESIGNER and when I simulated there, I see +5VDC and +12VDC values. When I simulate on PSpice I see the approximately correct output for +5VDC. But for +12VDC, I still see approximately +5VDC. I want to know the source of the problem here. I do not want to encounter similar problems when I purchase the product. I would like your support in this matter.