This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-010056: TIDA-010056

Can you provide equation to DC-link capacitance for inverter or bldc motor driver ?

  • Hi,

    The capacitance of dc-link capacitor depend on many factors as below,
    1. Capacitor material and type
    2. Ripple current on capacitor
    3. Temperature range, temperature profile, cooling
    4. Input DC/AC ripple voltages, minimum input voltage
    5. Allowed ripple voltage and frequency
    6. Maximum power and current
    7. pwm frequency for inverter
    8. motor parameters, phase inductance

    You can refer to this formula to simple calculate the capacitance C = Vbus / (32 ∗ L ∗ ΔV ∗ fpwm^2), the ΔV depends on voltage and current ripple, power.Or you can start with a 1W~1uF electrolytic capacitor.

    Actually, this is a complex question, you can search more paper or thesis from website.

    Thanks!

    Jenson