Part Number: TIDA-00555
Other Parts Discussed in Thread: TMDSCNCD28P65X, TL082H, TMDSHSECDOCK
Tool/software:
Looking for voltage and current measurement evaluation boards (not IC chip only such as TL082H that requires soldering). I already bought one TMDSCNCD28P65X and the docking station - TMDSHSECDOCK. And now I need peripheral for voltage and current measurements.
Voltage and current be measured as follows:
- AC Voltages : 3 Phase 690V L-L
- DC Voltage: 0 - 1300V
- Current range: 0 – 300A
Challenges: I cannot connect high voltages directly on the MCU (TMDSCNCD28P65X).
Background: In the past, I used TI references for a PCS block diagram to find the right module, which provided a recommendation. However, upon purchase, I only received the IC chip – which was not useful as it needed soldering.
www.ti.com/.../power-conversion-system-pcs
Any recommendation for the above???
Thank you.