This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-01292: TIDA-01292

Part Number: TIDA-01292
Other Parts Discussed in Thread: TIDA-010938, TIDA-010933

Tool/software:

I am working on low-frequency off-line UPS DC-AC converter design.

So, can I know part number of Transformer and also get the datasheet?

which TI uses in this design (TIDA-01292).

  • Hi, 

    You may see TIDA-010292 is a power design for low frequency offline UPS. It has a lot of design considerations and calculations on FET driver, sensing, control, etc. While the transformer is a normal 850VA 50/60Hz transformer which we didn't put a lot documents. I tried to reach out to the designer but seems he left. To better support you, you may look at below more designs: 

    TIDA-010938; TIDA-010933 both are common used in energy storage systems. 

    Thanks.

    Ryan