Part Number: PMP21455
Other Parts Discussed in Thread: PMP20708, UCC28881
Tool/software:
Hi,
We're designing a very compact mains powered device, and the PMP21455 specs and small form factor fit our requirements.
I've have some questions in regards to reducing the size and the amount of necessary components:
1. Are the rectification components for the unused 24V output necessary? Can we leave this secondary winding floating or just place a small loading resistor across it?
2. Can we use the same approach as in the 24V PMP20708 design variant, where the auxiliary winding is used for output voltage regulation instead of an optocoupler solution?
3. If I understood correctly, the Q1 and R7 are used instead of the internal regulator of the UCC28881 to extend the operating input voltage below 30VDC? I assume that's the main reason that 2 large 8.2uF capacitors are used for primary smoothing.
Since we're designing our device to operate with either universal mains or perhaps 240VAC only, can smaller values be used for C3 and C4 in this case? Any suggestions are appreciated.
Also, we'd be interested in approaches to fix/mitigate the high output voltage under no/small load conditions (From the test report: 5.4V with no load, 4.6V under load).
Thanks in advance, and sorry for the long post.
Regards,
Lazar