Part Number: PMP8740
Other Parts Discussed in Thread: PMP30092, , UCC28950
Tool/software:
Hi,
Need help in impementing the following requirements. For the reference boards I saw the PMP8740 that can provide the required outputs. Can I change the output voltage to 100VDC, is it programatically controlled. What other changes do I need to make in order to get the required output voltage? Secondly I don't need the LCD and buttons as this one will be a regular AC-DC supply without battery charging requirements... Also I believe the same PFC can be used to generate 24VDC as well following PMP30092 reference design then further voltage branches can be acheived by using buck regulators from it.