Other Parts Discussed in Thread: LMR38025, LMR38020EVM
Tool/software:
Hi,
I’m currently working on designing DC/DC buck converter to step down 24 V input voltage to 15 V.
Simulating transient response I get great results when converter is loaded with higher current approx. 400 mA or higher, not sure of the exact value. But when lightly loaded like 10 mA, 100 mA, I get this weird “startup” behavior. After some time everything goes back to normal. Can somebody please explain this behavior, is converter unstable? What should I do?
I’m attaching pspice schematic and simulation responses.
I have another question which is less important but it would be nice to know.
How likely or is it even possible to obtain values of internal compensation components like gain of the EA, Rc, Cc of internally compensated PCM converters e.g. LMR38025?
Thanks and best regards,
Ivan