Other Parts Discussed in Thread: UCC28180
Tool/software:
Dear TI Support Team,
I hope this message finds you well. I am currently working on implementing the TIDA-00776 350W reference design for a PFC circuit, but I am encountering a critical issue that I hope you can help me resolve.
The problem I am facing is that the PFC IC burns out during operation, and the output voltage exceeds 550V, which is far beyond the expected range for this design. I am using an external 12V lab supply for the UCC28180, and my startup sequence involves first applying AC and then powering the 12V DC. Despite following this sequence, the board is not functioning as expected.
Additionally, I have set the Vsense voltage to 5V in the circuit, which is intended to correspond to an output voltage of 400V. However, the circuit is still producing a much higher output voltage than expected.
Could you please provide guidance on why this might be happening? Specifically:
- Is the startup sequence I am using potentially causing the issue?
- Could there be a problem with the feedback loop or overvoltage protection in the reference design?
- Are there any recommended troubleshooting steps or common pitfalls associated with using the TIDA-00776 reference board in this configuration?
I would greatly appreciate any insights or recommendations to prevent the IC failure and correct the overvoltage problem.
Best Regards,
Mohd Sahid