LM5146-Q1: LM5146-Q1

Part Number: LM5146-Q1
Other Parts Discussed in Thread: LM5146

Tool/software:

i want to make sure that my designis correct to output 12.3V at 5A 

  • Hi firas,

    This looks pretty good. Please complete the LM5146 quickstart calculator, so we can review component selection (particularly the compensation). Also, please confirm the FET part numbers.

    The specs here are quite similar to that of the LM5146 EVM, which is 12V, 8A, 400kHz.

    Regards,

    Tim