Other Parts Discussed in Thread: LM5146,
Tool/software:
Hello team,
I'm Using LM5146Q1 in one of my applications. Input ranges from 35V to 54V, Output is 12V, 10A. I have designed the converter and during no load im getting the output voltage as 12. When I started loading the minimum load (around 50mA) also the output voltage is dipping to 5~6V. I'm using MOSFET Rds(11mOhms) on for the current sensing purpose & Rlimit=634 Ohms. Could you please help me on this.
Regards,
Kumar