This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-010015: Request specifications for magnetic elements L1, L6, L7, and T1

Part Number: TIDA-010015

Tool/software:

hello

I have an inquiry regarding TIDA-010015.

When manufacturing a product, “L1, L6 , L7, T1” are identified as parts that need to be manufactured.

- L1, L6 : Transformer, 160 uH, TH
- L7 : Inductor, Ferrite, 330 µH, 6.1 A, 0.074 ohm, TH
- T1 : PQ3230(Payton)/Transformer, TH

Please provide the data (Datasheet or Specification) with the core, bobbin, wire thickness, and turn ratio required to make the above magnetic elements.