This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-01352: broken archive file TIDRRK7.ZIP (6527 K)

Part Number: TIDA-01352
Other Parts Discussed in Thread: TIDA-01371

Tool/software:

Dear Sir or Madam,
The following archive is broken on your server.
The downloaded file size is correct 6527 K, but I receive an error message during unzipping and I cannot convert the project from Altium binary to ASCII and next to OrCAD.
TIDRRK7.ZIP (6527 K)

Files used for 3D models or 2D drawings of IC components

Please fix an archive or help with conversion to OrCAD.

I can convert TIDA-01371 to OrCAD without any problem.