This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

POWERSTAGE-DESIGNER: Power Stage Designer 5.0 FET selection sorting bug

Part Number: POWERSTAGE-DESIGNER


Tool/software:

The 'Select FET' window pops up on clicking the 'Load' button in the 'FET Losses Calculator'. The various columns can be sorted by clicking the column header but it sorts them alpha-numerically rather than numerically. This leads, for example, to the sort order for the start of the COSS list showing 101,1060,1080,1100,1160, 1160,130,136 etc.

[Edit] Obviously the Fet part number and package types columns should remain to be sorted alpha-numerically!

This is very unhelpful when selecting FETs by parameters but should be easy to fix.

Regards,

   Tony H