Part Number: PMP22343
Tool/software:
Hi.
I have built a +/- 30V PSU following suggested PMP22343 design following the specs rules however I get a very noisy output but what is worst the waveform is oscillating in a sort of manner.
Here attached the schematic:

I have tried to use same layout with 4 layer ground planes with sufficient vias

however during tests (used a 0,125mA LOAD as suggested by the TIDT158.PDF test reports provided) I got following problems:
- Comparing to the test output voltage ripple is higher due to spikes on the positive and negative waveform at the output caps
VDD:

VSS: even worser

- The switching frequency is constantly oscillating between 149 and 151 kHz.
- Primary switching node at D2 shows some sort of ringing (?) (input is +12V).
At no load applied the voltage is following:

sometimes it gets worse:

here at 125mA output:

here at 300mA output:

- Same for Primary Switching Node D1

- But what is worse is that the waveform observed ad D1 and D2 are constantly going back and forth in an oscillating manner. Here a magnification of the voltage:
Oscillation:

Magnification 1:

Magnification 2:

Magnification 3:

- Finally the spectrum analysis of the output voltage of both VDD and VSS rails shows a huge harmonics of the 150kHz switching frequency:
VDD:

VSS:

Could You please help me find out what is going on?
best regards and thanks.
Steve