This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-01187: Un expected behavior of Reference design on TINA

Part Number: TIDA-01187
Other Parts Discussed in Thread: TLV3601, OPA857, THS4541, OPA855, OPA856

Tool/software: TINA

HI

I adopted the TIDA01187 reference for my input signal from photo diode to TTL conversion

Signal nature PW is 100nS and rise time of 1nS, Pulse rep rate can be from 1Hz to 20MHz, i need to give out this from photo diode to TTL output.

below is the approach

What iam seeing is some convergence issue on tool why does this happen,  i am attaching the design file of TINA

What i wish to do is use this stage for TTL output at 5V , doing that also throws an error.

so my intial query is to get of this issue first.post which i want to create a LoS indicator which can indicate a TTL out of Loss of signal, before that the reference should go smooth in simulation

OPA857+THS4541+TLV3601.TSC