This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-01606: about sfra question?

Part Number: TIDA-01606
Other Parts Discussed in Thread: SFRA,

Tool/software:

Hi
Ask some questions about SFRA.
Follow TIDA-01606_userGuide to do Lab6 experiments
The hardware installation is approximately as follows:
Chroma Regenerative Grid Simulator(61815) AC source -> tida-01606 -> chrome Bidirectional DC power Supply(62180D-1200) DC Load

1. tida-01606 -> The load is set to 3.18K resistor
2. AC source +30Vrms -> tida-01606
3. TINV_allRelaySet -> 1
4. TINV_allRelaySet -> -0.013
5. TINV_startPowerStage -> 1
6. AC source change to 180Vrms(or 220Vrms) -> tida-01606

Test SFRA.
Question 1. Why are the results of each test different? There is a huge difference?
Like the picture below, will there be a peak close to 120dB? What does this mean? Can you explain it to me?
Because in other graphs it is downward close to 120dB?

Question 2: When working on Compensation Designer, there will be a red dot in the graph. What does it mean? Should its position be close to 0dB? Because sometimes the red dot cannot be seen?
Sorry to trouble you, thank you

  • Gavin,

    The red dot is the location of the zero fz0.  It affects your compensation response.  the red dot should move when you edit the fz0 in the compensation designer gui.

    -Kelvin

  • Gavin,

    I haven't tested the SFRA myself so i'm not sure about that tool.  In the future, i think this feature will not be supported in the SDK.

    About the repeatability part,  if were you i would make sure to perform the test at a stable working condition.  Based on your compensation designer, there is a weird spike close to 400Hz.  try to get your system to a a nice phase response in the passband.  you should try to reduce your Folg_cf frequency to increase stability.

  • Hi,
    Okay, I will try again based on your suggestion.
    Also, I would like to ask, if the SDK does not support SFRA in the future, are there other methods or tools to adjust the Kp/Ki value?
    BR,
    Gavin